This document introduces the demo project of "go_power_status", including how to get the battery percentage and power status.
Content
IDE Preperation
Software
- Visual Studio 2010 SP1
- Slamware Windows SDK:Slamware Windows SDK
- RoboStudio(for map display):Robostudio installer
Sample Code:
Higher version of Visual Studio will cause errors. Sometime you will need to upgrade SP1 package to make your VS compatable with .Net Framework.
Hardware
(Either one of following)
- Slamware SDP mini
- Slamware SDP
- Slamware Kit
- Zeus/Apollo robot base
Download
Compiling
- Right click on "get_power_status" project, set as StartUp project.
Right click on "get_power_status", then " Properties",configure "include" and "lib" directories to the corresponding folder path of Slamware SDK.
It's not necessary to copy files to the project directory, user will only need to configure the path of SDK.
- Right click on " get_power_status ", then "properties",set "Command Arguments" as follows:
Syntax :get_power_status <IP address>> - Click " F5" to execute.
- The output from console will be as follows:
Code
get battery percentage and power status
获取电量/充电状态SlamwareCorePlatform sdp = SlamwareCorePlatform::connect(argv[1], 1445); std::cout <<"SDK Version: " << sdp.getSDKVersion() << std::endl; std::cout <<"SDP Version: " << sdp.getSDPVersion() << std::endl; PowerStatus status = sdp.getPowerStatus(); std::cout << "Battery Percentage: " << status.batteryPercentage << std::endl; std::cout << "is Charging: " << status.isCharging << std::endl; std::cout << "is DC connected: " << status.isDCConnected << std::endl; if(status.dockingStatus == DockingStatusNotOnDock) std::cout << "Docking status: Not on dock" << std::endl; else if(status.dockingStatus == DockingStatusOnDock) std::cout << "Docking status: On dock" << std::endl; else std::cout << "Docking status: Unknown" << std::endl;