本页介绍了Speed regulation的用法, 如何调用setsystemparameter()接口调节机器人速度。
本页内容
运行环境准备
软件平台
- Visual Studio 2010 SP1
- Slamware Windows SDK:Slamware Windows SDK
- RoboStudio(用于显示地图):Robostudio installer
Sample Code:
使用更高版本的Visual Studio可能会带来编译异常。
使用Visual Studio 2010(无SP1)可能会因为无法与.Net Framework兼容而报编译错误,此时增加SP1更新包即可解决问题
硬件平台
(以下任选其一)
- Slamware SDP mini
- Slamware SDP
- Slamware 套装 (基于Slamware导航方案的用户机器人系统)
- Zeus/Apollo等底盘系统
例程下载
编译运行
- 打开samples工程,右键Speed regulation, 将此工程设置成StartUp project
右键speed_regulation, 打开属性选项,将Slamware SDK 的include目录和lib目录添加到工程
Slamware SDK的include和lib目录无需复制到参考例程目录,只需在Visual Studio里指定路径即可。
- 右键speed_regulation, 在Debugging页面中command Arguments处输入 192.168.11.1
格式说明:speed_regulation <IP address> - 点击F5运行
- 可以连上Robostudio查看地图及机器人的运动
代码描述
机器人会以低中高三档速度运动在三角形三边循环运动,其速度分别对应0.3m/s,0.4m/s,0.5m/s
调节速度SlamwareCorePlatform sdp = SlamwareCorePlatform::connect(ip_address, 1445); std::cout <<"SDK Version: " << sdp.getSDKVersion() << std::endl; std::cout <<"SDP Version: " << sdp.getSDPVersion() << std::endl; rpos::actions::MoveAction action = sdp.getCurrentAction(); rpos::core::Location location1(1,0); rpos::core::Location location2(-1,0); rpos::core::Location location3(0,1.414); while (true) { if (action) action.cancel(); action = sdp.moveTo(location1, false,true); if (action.getStatus() == rpos::core::ActionStatusError) std::cout << "Action Failed: " << action.getReason() << std::endl; bool bRet2 =sdp.setSystemParameter(SYSPARAM_ROBOT_SPEED, SYSVAL_ROBOT_SPEED_HIGH); std::cout <<"Robot is moving to: (" << location1.x() <<" , "<<location1.y()<<") on speed"<< " HIGH( 0.5m/s )" << std::endl; action.waitUntilDone(); action = sdp.moveTo(location2, false,true); if (action.getStatus() == rpos::core::ActionStatusError) std::cout << "Action Failed: " << action.getReason() << std::endl; bool bRet3 =sdp.setSystemParameter(SYSPARAM_ROBOT_SPEED, SYSVAL_ROBOT_SPEED_LOW); std::cout <<"Robot is moving to: (" << location2.x() <<" , "<<location2.y()<<") on speed"<< " LOW( 0.3m/s )" << std::endl; action.waitUntilDone(); action = sdp.moveTo(location2, false,true); if (action.getStatus() == rpos::core::ActionStatusError) std::cout << "Action Failed: " << action.getReason() << std::endl; bool bRet1 =sdp.setSystemParameter(SYSPARAM_ROBOT_SPEED, SYSVAL_ROBOT_SPEED_MEDIUM); std::cout <<"Robot is moving to: (" << location3.x() <<" , "<<location3.y()<<") on speed"<< " MEDIUM( 0.4m/s )" << std::endl; action.waitUntilDone(); }