You are viewing an old version of this page. View the current version.

Compare with Current View Page History

« Previous Version 3 Next »



This document introduces the demo project of "move_to_spot", including how to move in standard mode and virtual track mode.

Content


IDE Preparation 

  • Software

    • Visual Studio 2010  SP1
    • Slamware Windows SDK:Slamware Windows SDK
    • RoboStudio(for map display):Robostudio installer 
    • Sample Code: 

      Higher version of Visual Studio will cause errors. sometime you will need to upgrade SP1 package to make your VS compatable with .Net Framework.

  • Hardware

          (Either one of following)

    • Slamware SDP mini 
    • Slamware SDP
    • Slamware Kit 
    • Zeus/Apollo robot base

Download

Win32-Demo

Compiling

  1. Right click on "move_to_spot" project, set as StartUp project.
  2. Right click on "move_to_spot",then " Properties",configure "include" and "lib" directories to the corresponding folder path of Slamware SDK.

    It's not necessary to copy files to the project directory, user will only need to configure the path of SDK.


  3. Right click on "move_to_spot",set "Command Arguments"  as follows:
    Syntax Description:move_to_spot <IP address> 



  4. Click " F5" to execute.
  5. Robot motion and map could be seen on Robostudio.

Code 

  • Robot moves firstly navigate to point(2, 0) in standard mode, and then back to point (0,0) in virtual track mode, if any obstacle is detected, it will be automatically avoided during the motion.

    导航到目标点
            SlamwareCorePlatform sdp = SlamwareCorePlatform::connect(argv[1], 1445);
    		std::cout <<"SDK Version: " << sdp.getSDKVersion() << std::endl;
    		std::cout <<"SDP Version: " << sdp.getSDPVersion() << std::endl;
    		rpos::actions::MoveAction action = sdp.getCurrentAction();
    		if (action)
    			action.cancel();		
    		//move to location (2, 0), not on virtual track
    		rpos::features::motion_planner::MoveOptions options;
    		options.flag = MoveOptionFlag(MoveOptionFlagMilestone | MoveOptionFlagPrecise);
    		action = sdp.moveTo(rpos::core::Location(2, 0), options);
    		action.waitUntilDone();
    		if (action.getStatus() == rpos::core::ActionStatusError)
    			std::cout << "Action Failed: " << action.getReason() << std::endl;
    		//draw a virtual track from (0, 0) to (2, 0), then move to (0, 0) via virtual track
    		rpos::core::Line line(rpos::core::Point(0,0),rpos::core::Point(2,0));
    		sdp.addLine(ArtifactUsageVirtualTrack, line);
    		options.flag = MoveOptionFlag(MoveOptionFlagKeyPoints | MoveOptionFlagPrecise);
    		action = sdp.moveTo(rpos::core::Location(0, 0), options);
    		action.waitUntilDone();
    		if (action.getStatus() == rpos::core::ActionStatusError)
    			std::cout << "Action Failed: " << action.getReason() << std::endl;
  • No labels