本页介绍了move_to_spot的用法, 包含导航模式下和轨道模式下的运动到目标点的过程
本页内容
需要
软件平台
- Visual Studio 2010
- Slamware Windows SDK:Slamware Windows SDK
- RoboStudio:Robostudio installer
- Sample Code:
硬件平台
(以下任选其一)
- Slamware SDP mini
- Slamware SDP
- Slamware 套装 (基于Slamware导航方案的用户机器人系统)
- Zeus/Apollo等底盘系统
编译运行
- 打开samples工程
- 右键move_to_spot, 打开属性选项,将Slamware SDK 的include目录和lib目录添加到工程
- 右键move_to_spot, 将此工程设置成StartUp project
- 右键move_to_spot, 在Debugging页面中command Arguments处输入 192.168.11.1
格式说明: move_to_spot <IP address> - 点击F5运行
- 可以连上Robostudio查看地图及机器人的运动(TODO 添加RoboStudio的视频)
代码描述
代码功能说明: 机器人导航运动到(2, 0) 点,然后从(2,0) 沿虚拟轨道运动到(0, 0)点
导航到目标点SlamwareCorePlatform sdp = SlamwareCorePlatform::connect(argv[1], 1445); std::cout <<"SDK Version: " << sdp.getSDKVersion() << std::endl; std::cout <<"SDP Version: " << sdp.getSDPVersion() << std::endl; rpos::actions::MoveAction action = sdp.getCurrentAction(); if (action) action.cancel(); //move to location (2, 0), not on virtual track rpos::features::motion_planner::MoveOptions options; options.flag = MoveOptionFlag(MoveOptionFlagMilestone | MoveOptionFlagPrecise | MoveOptionFlagWithYaw | MoveOptionFlagReturnUnreachableDirectly); action = sdp.moveTo(rpos::core::Location(2, 0), options, pi/2); action.waitUntilDone(); if (action.getStatus() == rpos::core::ActionStatusError) std::cout << "Action Failed: " << action.getReason() << std::endl; //draw a virtual track from (0, 0) to (2, 0), then move to (0, 0) via virtual track rpos::core::Line line(rpos::core::Point(0,0),rpos::core::Point(2,0)); sdp.addLine(ArtifactUsageVirtualTrack, line); options.flag = MoveOptionFlag(MoveOptionFlagKeyPoints | MoveOptionFlagPrecise | MoveOptionFlagReturnUnreachableDirectly); action = sdp.moveTo(rpos::core::Location(0, 0), options); action.waitUntilDone(); if (action.getStatus() == rpos::core::ActionStatusError) std::cout << "Action Failed: " << action.getReason() << std::endl;