Versions Compared

Key

  • This line was added.
  • This line was removed.
  • Formatting was changed.

...

a).Please kindly connect to the base hotspot(Name as Slamware-xxxxxx,AP mode)or connect to local wifi(STA Mode), enter the robot IP address on the browser (The defualt IP address is 192.168.11.1.AP mode), and check whether the device SN information is fully displayed.
Image Removed
Image Added
b). Check whether the USB3.0 usb hub or the typec cable of the base itself is connected correctly. If necessary, replug and test.
c).If the above cannot solve the issue, please kindly contact Slamtec for support.

...

45.The robostudio show " "magtape [x] triggered" error message

Image AddedImage Removed


a)Please check whether the application scenario is flat and there is no magnetic environment on the ground.
b)Please click Clear All and check if the message disappears.
c)If step b cannnot solve the issue, please kindly turn off the magnetic sensor in Robostudio. The specific operation is as follows:

  • Enter the robot ip in the robot window and connect the robot

  • Right-click the robot ip address and select robot details

  • Select the sensors page, find the MagneticTapeDetector, right-click on status, and you can choose to disable always.


Image AddedImage Removed

46.How to use the Precision Camera(QR Camera)

...

After connecting the platform in robostudio, select motion strategy in the debug menu. After entering Motion strategy, you can use different strategies or enter the required speed in customized (speed range 0.1~ 1.5m/s).


Image RemovedImage Added

Image RemovedImage Added


Note: Before changing the paltform speed, you need to click Pause Mapping in SLAM Menu
Image RemovedImage Added

51.How to adjust the screen orientation when using the Slamtec Base/Robot

...