Versions Compared

Key

  • This line was added.
  • This line was removed.
  • Formatting was changed.

...

  1. 在sample code所在文件夹中,打开 samples.sln
  2. 右键go_home_to_charge, 打开属性选项,将Slamware SDK 的include目录和lib目录添加到工程
  3. 右键go_home_to_charge, 将此工程设置成StartUp project
  4. 右键go_home_to_charge, 在Debugging页面中command Arguments处输入 192.168.11.1 (Slamware AP 模式默认IP地址)。 注: 此sample为 windows console application, 也可以在console中用命令行执行,用法为:go_home_to_charge <IP address> 
  5. 点击F5运行
  6. Console输出为(下图中0, 1两个bumper是触发状态,为0)
    Image Removed


描述:

  • 代码功能说明: 获取电量/充电状态调用goHome()接口来进行自动回充,如果没有找到充电桩或者充电失败,会重复至多三次调用goHome()

    Code Block
    languagecpp
    firstline1
    title获取传感器数据
    linenumberstrue
            const int max_go_home_times = 3;     	
            SlamwareCorePlatform sdp = SlamwareCorePlatform::connect(argv[1], 1445);
            std::cout <<"SDK Version: " << sdp.getSDKVersion() << std::endl;
            std::cout <<"SDP Version: " << sdp.getSDPVersion() << std::endl;
    		int go_home_count = 1;
    		rpos::actions::MoveAction action;
    		do {
    			action = sdp.goHome();
    			action.waitUntilDone();
    			if(action.getStatus() == rpos::core::ActionStatusFinished)
    				break;
    			std::cout << "go home to charge times count: "  << go_home_count << std::endl;
    			go_home_count++;
    		}
    		while(go_home_count <= max_go_home_times);
    


...