Excerpt |
---|
本页介绍了get_sensor_value的用法, 包含当前所有传感器的类型,安装位置,触发状态等。 |
本页内容
Table of Contents |
---|
运行环境准备
软件平台
需要:
...
- Visual Studio 2010 SP1
- Slamware Windows SDK:
...
- Slamware Windows SDK
- RoboStudio(用于显示地图):Robostudio installer
Sample Code:
硬件平台:
Info 使用更高版本的Visual Studio可能会带来编译异常。
使用Visual Studio 2010(无SP1)可能会因为无法与.Net Framework兼容而报编译错误,此时增加SP1更新包即可解决问题
硬件平台
(以下任选其一)
- Slamware SDP mini
...
- Slamware 套装 (基于Slamware导航方案的用户机器人系统)
...
- Apollo/Ares/
...
- Athena等底盘系统
编译运行:
准备工作: 开启机器人系统电源,雷达转动之后代表系统已经成功启动。
...
...
- _sensor_value,
...
- 将此工程设置成StartUp project
右键get_sensor_value,
...
打开属性选项,将Slamware SDK 的include目录和lib目录添加到工程
Info Slamware SDK的include和lib目录无需复制到参考例程目录,只需在Visual Studio里指定路径即可。
- 右键get_sensor_value,
...
- 在Debugging页面中command Arguments处输入 192.168.11.
...
- 1
格式说明:get_sensor_value <IP address> - 点击F5运行
- Console输出为(
...
- 下图中,
...
- sensor id为 1的bumper是触发状态,值为0)
...
...
代码描述
代码功能说明:
...
获取传感器数据
Code Block language cpp firstline 1 title 获取传感器数据 linenumbers true
...
SlamwareCorePlatform sdp = SlamwareCorePlatform::connect(
...
ip_address, 1445);
...
std::cout <<"SDK Version: " << sdp.getSDKVersion() << std::endl;
...
std::cout <<"SDP Version: " << sdp.getSDPVersion() << std::endl;
...
...
std::vector<ImpactSensorInfo> sensors;
...
bool result = sdp.getSensors(sensors);
...
if (result)
...
{
...
for (std::vector<ImpactSensorInfo>::iterator it = sensors.begin();
...
it != sensors.end(); ++it) {
...
std::cout << "Sensor id : " << it->id << std::endl;
...
if (it-
...
>coreSensorType ==
...
SensorTypeBumper)
...
std::cout << "Sensor
...
coreSensorType: Bumper" << std::endl;
...
else if (it-
...
>coreSensorType ==
...
SensorTypeCliff)
...
std::cout << "Sensor
...
coreSensorType: Cliff" << std::endl;
...
else if (it-
...
>coreSensorType ==
...
SensorTypeSonar)
...
std::cout << "Sensor
...
coreSensorType: Sonar" << std::endl;
...
else if (it->coreSensorType == SensorTypeMagTapeDetector) std::cout << "Sensor coreSensorType: MagTapeDetector" << std::endl; else return 1;
...
if (it->type == ImpactSensorTypeAnalog)
...
std::cout << "Sensor Type: Analog" << std::endl;
...
else if (it->type == ImpactSensorTypeDigital)
...
std::cout << "Sensor Type: Digital" << std::endl;
...
else return 1;
...
std::cout << "Sensor Position: ( " << it->pose.x() << " , " << it->pose.y() << " , " <<
...
it->pose.z() << " ) ; Yaw = " << it->pose.yaw() << std::endl;
...
ImpactSensorValue value;
...
sdp.getSensorValue(it->id, value);
...
std::cout << "Sensor Value : " << value.value<< std::endl; std::cout<<std::endl; } }