本页介绍了get_sensor_value的用法, 包含当前所有传感器的类型,安装位置,触发状态等。 |
本页内容
Sample Code:
使用更高版本的Visual Studio可能会带来编译异常。 使用Visual Studio 2010(无SP1)可能会因为无法与.Net Framework兼容而报编译错误,此时增加SP1更新包即可解决问题 |
(以下任选其一)
右键get_sensor_value, 打开属性选项,将Slamware SDK 的include目录和lib目录添加到工程
Slamware SDK的include和lib目录无需复制到参考例程目录,只需在Visual Studio里指定路径即可。 |
代码功能说明: 获取传感器数据
SlamwareCorePlatform sdp = SlamwareCorePlatform::connect(ip_address, 1445); std::cout <<"SDK Version: " << sdp.getSDKVersion() << std::endl; std::cout <<"SDP Version: " << sdp.getSDPVersion() << std::endl; std::vector<ImpactSensorInfo> sensors; bool result = sdp.getSensors(sensors); if (result) { for (std::vector<ImpactSensorInfo>::iterator it = sensors.begin();it != sensors.end(); ++it) { std::cout << "Sensor id : " << it->id << std::endl; if (it->coreSensorType == SensorTypeBumper) std::cout << "Sensor coreSensorType: Bumper" << std::endl; else if (it->coreSensorType == SensorTypeCliff) std::cout << "Sensor coreSensorType: Cliff" << std::endl; else if (it->coreSensorType == SensorTypeSonar) std::cout << "Sensor coreSensorType: Sonar" << std::endl; else if (it->coreSensorType == SensorTypeMagTapeDetector) std::cout << "Sensor coreSensorType: MagTapeDetector" << std::endl; else return 1; if (it->type == ImpactSensorTypeAnalog) std::cout << "Sensor Type: Analog" << std::endl; else if (it->type == ImpactSensorTypeDigital) std::cout << "Sensor Type: Digital" << std::endl; else return 1; std::cout << "Sensor Position: ( " << it->pose.x() << " , " << it->pose.y() << " , " << it->pose.z() << " ) ; Yaw = " << it->pose.yaw() << std::endl; ImpactSensorValue value; sdp.getSensorValue(it->id, value); std::cout << "Sensor Value : " << value.value<< std::endl; std::cout<<std::endl; } } |