Versions Compared

Key

  • This line was added.
  • This line was removed.
  • Formatting was changed.

...

  1. 在sample code所在文件夹中,打开 samples.sln
  2. 右键configure_network_demo, 打开属性选项,将Slamware SDK 的include目录和lib目录添加到工程
  3. 右键configure_network_demo, 将此工程设置成StartUp project
  4. 点击F5运行
  5. 或编译之后在debug目录下用命令行运行configure_network_demo, 用法如下:

    configure_network_demo  [OPTS]   <SDP IP Address>
    slamware_address            The ip address string of the SLAMWARE SDP.
    AP                                     Configurate network in AP mode.
    STA                                   Configurate network in STA mode.
    --disable-dhcp                   disable dhcp.
    --enable-dhcp                   enable dhcp.
    --disable-wifi                     disable wifi
    -h                                      Show this message

  6. 在AP模式下配置网络参数,配置之后,wifi名称,密码, IP地址,信道,都会变成下图所设置数值
    Image Added
    此时,重新连接wifi名为test,密码为12345678的slamware AP之后, 可以用192.168.11.101连接slamware模块(192.168.11.1 为默认值,依然可用)
    Image Added
    此时wifi信道已经更改成6:
    Image Added
  7. 在station模式下配置网络,配置时需要输入当前可用局域网的名称和密码,成功之后,机器人将接入局域网,需要用机器人分到的IP来连接。
    Image Added
  8. 此时,将客户端连入同一个局域网,就可以访问slamware模块了。下图中,机器人分到的IP地址为:10.0.129.75
    Image Added