1.RS does not have a Lidar icon or the plugin cannot be installed?
Please download the offline version of RS. from the official website httpsRobostudio from the overseas help center (Topic 1.06). https://bucket-downloadwiki.slamtec.com/wordpress/RoboStudio%20v1.7.5_rtm.rar display/SD/Overseas+Help+Center
2.RS cannot be connected to a Lidar with a
...
USB adapter board
a).Check whether the serial port driver is installed in Device Manager. You can find the driver compressed file in the \rplidar_sdk\tools\cp2102_driver directory, and select the installation file according to your operating system after extraction: 64-bit operating systems use CP210xVCPInstaller_x64 files to install drivers, 32-bit operating systems use CP210xVCPInstaller_x86 files to install drivers.
b).Check whether the serial port adapter board is used correctly, and replace the serial port adapter board for testing.
- Black housing without DIP switch 1000000:S2: 1000000,S3
- No housing, no DIP switch 115200: A1M8
No housing, no DIP switch 460800:C1
- The black housing has DIP switches 115200: A2M8, A2M6
- Black housing with DIP switches 256000: A2M7, A2M12, A3, S1
- Note: A few years ago, the serial port adapter boards were all DIP switches, and the baud rate was 115200.
...
d).Check if there are other serial port tools connected to the Lidar at the same time, and the Lidar cannot be opened by two serial port tools at the same time.
e). Check whether the Lidar serial port line is in good contact, you can remove the bottom cover to see if the serial port line comes off.
f).Overvoltage protection prevents the Lidar from starting, and the supply voltage is between9V and 5.2V. The overvoltage protection values can be tested using the wiring method below.
g).If the above is normal, it means that the serial port of the Lidar circuit board is damaged or broken, it needs to be returned to the factory for repair. RS cannot be connected to a Lidar with a network port accessory board.If the above cannot help to solve the issue, please kindly contact Slamtec for support. If it is necessary, the lidar needs to be sent back for analysis.
3.RS cannot be connected to a Lidar with a network port accessory
...
board
a)Check whether the IP address of the network port accessory board can be pinged, and if it cannot be pinged, check whether the IP address of the local machine is set to the same network segment. You can also restore to the factory settings by pressing the button, and the button near the Lidar power port can initialize the accessory board, after initialization, you need to reflash the firmware and set up a new IP. Check whether the network port accessory board is used correctly.
- Network port accessory board 115200: A2M8, A2M6
- Network port accessory board 256000: A2M7, A2M12, A3, S1
- Network port accessory board 1000000:S2,S3
- Note: The network port accessory board 115200 and the network port accessory board 256000 can be flashed with the corresponding version of firmware as needed to achieve the general purpose.
...
- Check to see if the power supply is between 9V and 28V.
- Check whether the IP address of the network port accessory board can be pinged, and if it cannot be pinged, check whether the IP address of the local machine is set to the same network segment.
- Early S2E Lidars may first power up the Lidar, and then power up the computer or industrial computer, resulting in the inability to pass the Lidar. In this case, you need to upgrade to the latest firmware.
5.Lidar ROS sdk under Ubuntu 22.04 humble version used abnormally?
Existing Lidars do not support Ubuntu 22.04, customers are advised to use Ubuntu 20.04Please kindly use the latest version ROS SDK from the overseas help center (Topic1.05):https://wiki.slamtec.com/display/SD/Overseas+Help+Center
6.Is the Lidar fog-proof or used in dense fog?
...
Insufficient Lidar voltage.
8.Whether the A series and S1 Lidars have a network port
...
adapter board
Apart from A1M8, other Lidars have corresponding network port accessory versionsadapter board, but use the network port accessory version adaper board corresponding to the Lidar baud rate.
...
14.“Internal error” occurs during Lidar operation
Plug and unplug the power cord and the USB cable of the USB adapter at the same time. Ensure that the two USBs are plugged and unplugged at the same time (within 3 seconds), and restart to check whether the power supply voltage meets the power requirements.If it is necessary, please kindly contact Slamtec for support.
15.There is no data on the Lidar under the Linux system
1.If it is a Linux system, check to see if the USB is authorized.
Check whether the USB is authorized (if the virtual machine needs to restart the serial port accessory board, select Connect to the virtual machine): ls -l /dev |grep ttyUSB
Licensed USB: sudo chmod 666/dev/ttyUSB0
2.Download and compile SDK from the official website. If there is still no data to check whether the local ROS is successfully installed, use the baby turtle to check whether the installation is successful.
3.Re-download and compile the ROS feature pack.
16.Common commands for serial port tools (A series Lidar)
...
float angle_max = DEG2RAD(360.0f);
After running the Lidar, use Rostopic HZ Scan to check that the frequency modification is successful.
...
In /S2ROS120221020/src/rplidar_ros-master/launch/, modify the rplidar_a3.launch file, and modify the respective mode at the bottom. ROS can be started to verify that the mode modification is successful.
19.How to use or download the SDK?
Please refer to the SDK user manual and SDK link from the overseas help center(Topic 1.04&1.05)https://wiki.slamtec.com/display/SD/Overseas+Help+Center
20.How to use the ROS SDK?
Please refer to the latest ROS SDK link and the ROS Tutorial from the overseas help center(Topic1.05&1.10)https://wiki.slamtec.com/display/SD/Overseas+Help+Center
21.How to make the lidar use with the Arduino?
Please refer to the lidar communication protocol and pinouts in the lidar datasheet,please download from the overseas help center(Topic 1.01&1.03):
https://wiki.slamtec.com/display/SD/Overseas+Help+Center .
And please refer to the S2 lidar sample library on Arduino:https://github.com/KKest/ESP-rplidarS2
Note:The baud rate for S2 is 1M. If you use another model lidar,please use the correct lidar baud rate.
Baud rate :1000000(1M):S2,S3
460800:C1
256000:S1,A3,A2M12,A2M7
115200:A2M8,A1M8
22.There is no data on the Lidar
Please provide the lidar SN number and test screenshot of the lidar under robostudio, and then contact our FAE for support.If it is necessary, the lidar needs to be sent back for analysis.
23.How to modify the ip of the lidar.
If the lidar is S2E/T1 model, please kindly refer to the user manual to modify the IP address. The user manual can be downloaded from the overseas help center (Topic 1.02):
https://wiki.slamtec.com/display/SD/Overseas+Help+Center
If using the network port adapter, please kindly contact Slamtec for support and provide the correct lidar model to slamtec.
- Network port accessory board 115200: A2M8, A2M6
- Network port accessory board 256000: A2M7, A2M12, A3, S1
- Network port accessory board 1000000:S2,S3
24.Where can download the protocol?
Please kindly download the protocol from the overseas help center(Topic1.03): https://wiki.slamtec.com/display/SD/Overseas+Help+Center
25.How to use the lidar with Raspberry Pie?
Please kindly refer to the SDK and protocol which can be downloaded from the overseas help center (Topic1.03,1.04&1.05): https://wiki.slamtec.com/display/SD/Overseas+Help+Center
It can support Ubuntu 16.04,18.04,20.04 and 22.04
26.How to use the lidar with Jeston Nano?
Please refer to the latest ROS SDK link from the overseas help center(Topic1.05)https://wiki.slamtec.com/display/SD/Overseas+Help+Center
27.How to use the RPLIDAR Interactive Toolkit
Please kindly refer to the RPLIDAR Interactive Material from the overseas help center(topic 1.09):https://wiki.slamtec.com/display/SD/Overseas+Help+Center
29.How to calculate the size of the object identifiable by lidar?
Object Length L=n×π×r/180 ,r is the distance value between the measured object and the lidar ,n is the minimum angle resolution,π≈3.14, the myopia arc length can be used as the minimum size of the measured object.
30.How to use the Ethernet module?
A Series Ethernet module config tool and guide.7z
S2 Ethernet moduel config tool and guide.7z