Versions Compared

Key

  • This line was added.
  • This line was removed.
  • Formatting was changed.
Excerpt

本页介绍了get_power_status的用法, 包含当前的充电状态,电池电量等。



本页内容

Table of Contents


运行环境准备

  • 软件平台

需要:

...

    • Visual Studio 2010  SP1
    • Slamware Windows SDK:

...

...

硬件平台:

    • Info

      使用更高版本的Visual Studio可能会带来编译异常。

      使用Visual Studio 2010(无SP1)可能会因为无法与.Net Framework兼容而报编译错误,此时增加SP1更新包即可解决问题

  • 硬件平台

          (以下任选其一)

      • Slamware SDP mini 

...

      • Slamware 套装 (基于Slamware导航方案的用户机器人系统)

...

      • Apollo/Ares/

...

      • Athena等底盘系统

编译运行:

      准备工作: 开启机器人系统电源,雷达转动之后代表系统已经成功启动。 

...



例程下载

Win32-例程下载


编译运行

  1. 打开samples工程,右键get

...

  1. _power_status,

...

  1. 将此工程设置成StartUp project
    Image Added

  2. 右键get_power_status,

...

  1. 打开属性选项,将Slamware SDK 的include目录和lib目录添加到工程

    Info

    Slamware SDK的include和lib目录无需复制到参考例程目录,只需在Visual Studio里指定路径即可。


    Image Added

  2. 右键get_power_status, 在Debugging页面中command Arguments处输入 192.168.11.

...

  1. 1 
    格式说明:get_power_status <IP address> 
    Image Modified

  2. 点击F5运行
  3. Console输出为

...


  1. Image Added


代码描述

  • 获取电量/充电状态

    Code Block
    languagecpp
    firstline1
    title获取电量/充电状态
    linenumberstrue
    		
            SlamwareCorePlatform sdp = SlamwareCorePlatform::connect(argv[1], 1445);
            std::cout <<"SDK Version: " << sdp.getSDKVersion() << std::endl;
            std::cout <<"SDP Version: " << sdp.getSDPVersion() << std::endl;
    		
    		PowerStatus status = sdp.getPowerStatus();
    		std::cout << "Battery Percentage: " << status.batteryPercentage << std::endl;
    		std::cout << "is Charging: " << status.isCharging << std::endl;
    		std::cout << "is DC connected: " << status.isDCConnected << std::endl;
    		
    		if(status.dockingStatus == DockingStatusNotOnDock)
    			std::cout << "Docking status: Not on dock" << std::endl;
    		else if(status.dockingStatus == DockingStatusOnDock)
    			std::cout << "Docking status: On dock" << std::endl;
    		else 
    			std::cout << "Docking status: Unknown" << std::endl;