Excerpt |
---|
This document introduces the demo project of "artifacts_demo", explaining user operation of Virtual Wall/Virtual Track, including how to add/delete/move modify artifacts. |
Content
Table of Contents |
---|
IDE Preparation
Software
- Visual Studio 2010 SP1
- Slamware Windows SDK:Slamware Windows SDK
- RoboStudio(for map display):Robostudio installer
Sample Code:
Info Higher version of Visual Studio will cause errors. sometime you will need to upgrade SP1 package to make your VS compatable with .Net Framework.
Hardware
(Either one of following)
- Slamware SDP mini
- Slamware SDP
- Slamware Kit
- Zeus/Apollo robot base
Download
Compiling
- Right click on "artifacts_demo" project, set as StartUp project.
Right click on "artifacts_demo", then " Properties",configure "include" and "lib" directories to the corresponding folder path of Slamware SDK.
Info Slamware SDK的include和lib目录无需复制到参考例程目录,只需在Visual Studio里指定路径即可。
- Right click on "artifacts_demo", then "properties",set "Command Arguments" as follows:
Syntax :artifacts_demo <IP address> - Click " F5" to execute.
- In robostudio, the output will be as follows:
Multimedia date // 虚拟轨道的删除、添加与移动 name bandicam 2017-12-13 18-21-31-346.mp4 - The output from console will be as follows:
- Delete one of the virtual tracks by selecting one of the IDs. the ID selected in the video is 3.
Code
- Delete all virtual tracks/walls.
Code Block | ||||||||
---|---|---|---|---|---|---|---|---|
| ||||||||
SlamwareCorePlatform sdp = SlamwareCorePlatform::connect(argv[1], 1445); std::cout << "Clearing existing tracks and walls..." << std::endl; sdp.clearLines(ArtifactUsageVirtualTrack); sdp.clearLines(ArtifactUsageVirtualWall); |
- add virtual walls
Code Block | ||||||||
---|---|---|---|---|---|---|---|---|
| ||||||||
std::cout << "Adding virtual walls..." << std::endl; std::vector<Line> walls; //add a 8 * 8 virtual wall square walls.push_back(Line(Point(-4, -4), Point(-4, 4))); walls.push_back(Line(Point(-4, 4), Point(4, 4))); walls.push_back(Line(Point(4, 4), Point(4, -4))); walls.push_back(Line(Point(4, -4), Point(-4, -4))); sdp.addLines(ArtifactUsageVirtualWall, walls); |
- add virtual tracks
Code Block | ||||||||
---|---|---|---|---|---|---|---|---|
| ||||||||
std::cout << "Adding virtual tracks..." << std::endl; std::vector<Line> tracks; //add a 2 * 2 virtual track square tracks.push_back(Line(Point(-1, -1), Point(-1, 1))); tracks.push_back(Line(Point(-1, 1), Point(1, 1))); tracks.push_back(Line(Point(1, 1), Point(1, -1))); tracks.push_back(Line(Point(1, -1), Point(-1, -1))); sdp.addLines(ArtifactUsageVirtualTrack, tracks); |
- modify a virtual wall ( similar with virtual wall modification)
Code Block | ||||||||
---|---|---|---|---|---|---|---|---|
| ||||||||
std::cout << "Moving vitual walls..." << std::endl; //sleep 5 seconds for displaying purpose only, not necessary boost::this_thread::sleep_for(boost::chrono::milliseconds(5000)); std::vector<Line> get_walls = sdp.getLines(ArtifactUsageVirtualWall); //shrink virtual wall square from 8 * 8 to 6 *6 for (std::vector<Line>::iterator it = get_walls.begin() ; it != get_walls.end(); ++it) { it->startP().x() *= 0.75f; it->startP().y() *= 0.75f; } sdp.moveLines(ArtifactUsageVirtualWall, get_walls); |
- Delete virtual tracks( similar with virtual wall deletion)
Code Block | ||||||||
---|---|---|---|---|---|---|---|---|
| ||||||||
std::cout << "Get all tracks..." << std::endl; std::vector<Line> get_tracks = sdp.getLines(ArtifactUsageVirtualTrack); for (std::vector<Line>::iterator it = get_tracks.begin() ; it != get_tracks.end(); ++it) { std::cout << "ID: " << it->id() << std::endl; std::cout << "Start from (" << it->startP().x() << " , " << it->startP().y() << ") " << "to (" << it->endP().x() << " , " << it->endP().y() << " ) " << std::endl; } std::cout << "Delete track by ID, please enter track ID:" << std::endl; int id; bool is_found = false; std::cin >> id ; for (std::vector<Line>::iterator it = get_tracks.begin() ; it != get_tracks.end(); ++it) { if (id == it->id()) { sdp.removeLineById(ArtifactUsageVirtualTrack, id); is_found = true; break; } } if(!is_found) std::cout << "Wrong ID" << std::endl; |