Versions Compared

Key

  • This line was added.
  • This line was removed.
  • Formatting was changed.

本页介绍了rotation_action_demo的用法, 包含顺时针旋转,逆时针旋转,旋转到指定角度等功能


本页内容

Table of Contents


运行环境准备

  • 软件平台

    • Visual Studio 2010  SP1
    • Slamware Windows SDK:Slamware Windows SDK
    • RoboStudio(用于显示地图):Robostudio installer
    • Sample Code: 

      Info

      使用更高版本的Visual Studio可能会带来编译异常。

      使用Visual Studio 2010(无SP1)可能会因为无法与.Net Framework兼容而报编译错误,此时增加SP1更新包即可解决问题


  • 硬件平台

          (以下任选其一)

      • Slamware SDP mini 
      • Slamware SDP
      • Slamware 套装 (基于Slamware导航方案的用户机器人系统)
      • Zeus/Apollo等底盘系统


例程下载

Win32-例程下载



编译运行

  1. 打开samples工程,右键rotation_action_demo, 将此工程设置成StartUp project


  2. 右键rotation_action_demo, 打开属性选项,将Slamware SDK 的include目录和lib目录添加到工程

    Info

    Slamware SDK的include和lib目录无需复制到参考例程目录,只需在Visual Studio里指定路径即可。



  3. 右键rotation_action_demo, 在Debugging页面中command Arguments处输入 192.168.11.1 
    格式说明:rotation_action_demo <IP address>


  4. 点击F5运行
  5. 可以连上Robostudio查看地图及机器人的运动
    Multimedia
    date//旋转到指定角度
    namebandicam 2018-01-30 16-13-28-334.mp4


代码描述

  • 机器人先逆时针转一周,再顺时针转一周,最后转到yaw值为pi的位置。

    Code Block
    languagecpp
    firstline1
    title旋转指定角度/旋转到指定角度
    linenumberstrue
     		SlamwareCorePlatform sdp = SlamwareCorePlatform::connect(argv[1], 1445);
            std::cout <<"SDK Version: " << sdp.getSDKVersion() << std::endl;
            std::cout <<"SDP Version: " << sdp.getSDPVersion() << std::endl;
    		rpos::actions::MoveAction action = sdp.getCurrentAction();
    		if (action)
    			action.cancel();			    
    		//anticlockwise rotation
    		rpos::core::Rotation rotation(pi*2, 0, 0);
    		action = sdp.rotate(rotation);
    		action.waitUntilDone();
    		std::cout << "Action Status: " << action.getStatus() << std::endl;
    		//clockwise rotation
    	    rotation.yaw() = pi * (-2);
    		action = sdp.rotate(rotation);
    		action.waitUntilDone();
    		std::cout << "Action Status: " << action.getStatus() << std::endl;
    		//rotate to a certain orientation
    		rpos::core::Rotation orientation(pi, 0, 0);
    		action = sdp.rotateTo(orientation);
    		action.waitUntilDone();
    		std::cout << "Action Status: " << action.getStatus() << std::endl;