This document introduces the demo project of “virtual_track_with_oa”, including a brief introduction to Virtual Track with OA Navigation mode. It can be understood as high-speed priority in road navigation. 1. Between the starting point and the target point, if there is a track, it will take precedence on the track. 2. If there are obstacles on the track, it will go off the track and then go on the track.
Content
IDE Preperation
Software
- Visual Studio 2010 SP1
- Slamware Windows SDK:Slamware Windows SDK
- RoboStudio(for map display):Robostudio installer
Sample Code:
Higher version of Visual Studio will cause errors. sometime you will need to upgrade SP1 package to make your VS compatable with .Net Framework.
Hardware
(Either one of following)
- Slamware SDP mini
- Slamware SDP
- Slamware Kit
- Zeus/Apollo robot base
Download
Compiling
- Right click on "virtual_track_with_oa" project, set as StartUp project.
Right click on "virtual_track_with_oa", then " Properties",configure "include" and "lib" directories to the corresponding folder path of Slamware SDK.
It's not necessary to copy files to the project directory, user will only need to configure the path of SDK.
- Right click on "virtual_track_with_oa", then "properties",set "Command Arguments" as follows:
Syntax :virtual_track_with_oa <IP address> - Click " F5" to execute.
- Robot's motion could be seen in Robostudio.
Code
Draw a 6-meter-long forward trajectory in the x-axis direction of the current position of the robot, and then walk along the trajectory to the target point.
Virtual Track with OA NavigationSlamwareCorePlatform sdp = SlamwareCorePlatform::connect(ip_address, 1445); std::cout <<"SDK Version: " << sdp.getSDKVersion() << std::endl; std::cout <<"SDP Version: " << sdp.getSDPVersion() << std::endl; //draw a 6 meter virtual track rpos::core::Pose sdp_pos = sdp.getPose(); rpos::core::Line line(rpos::core::Point(sdp_pos.x(), sdp_pos.y()),rpos::core::Point(sdp_pos.x() + 6, sdp_pos.y())); sdp.addLine(ArtifactUsageVirtualTrack, line); rpos::actions::MoveAction action = sdp.getCurrentAction(); if (action) action.cancel(); rpos::features::motion_planner::MoveOptions options; options.flag = MoveOptionFlag(MoveOptionFlagKeyPointsWithOA); action = sdp.moveTo(rpos::core::Location(0, 0), options); action.waitUntilDone(); if (action.getStatus() == rpos::core::ActionStatusError) std::cout << "Action Failed: " << action.getReason() << std::endl;;