You are viewing an old version of this page. View the current version.

Compare with Current View Page History

« Previous Version 14 Next »

本页介绍了move_to_spot的用法, 包含导航模式下和轨道模式下的运动到目标点的过程


本页内容



需要

软件平台

硬件平台

(以下任选其一)

  • Slamware SDP mini 
  • Slamware SDP
  • Slamware 套装 (基于Slamware导航方案的用户机器人系统)
  • Zeus/Apollo等底盘系统

编译运行

  1. 打开samples工程
  2. 右键move_to_spot, 打开属性选项,将Slamware SDK 的include目录和lib目录添加到工程
  3. 右键move_to_spot, 将此工程设置成StartUp project
  4. 右键move_to_spot, 在Debugging页面中command Arguments处输入 192.168.11.1 
    格式说明: move_to_spot <IP address> 
  5. 点击F5运行
  6. 可以连上Robostudio查看地图及机器人的运动


代码描述

  • 代码功能说明: 机器人导航运动到(2, 0) 点,然后从(2,0) 沿虚拟轨道运动到(0, 0)点

    导航到目标点
            SlamwareCorePlatform sdp = SlamwareCorePlatform::connect(argv[1], 1445);
    		std::cout <<"SDK Version: " << sdp.getSDKVersion() << std::endl;
    		std::cout <<"SDP Version: " << sdp.getSDPVersion() << std::endl;
    		rpos::actions::MoveAction action = sdp.getCurrentAction();
    		if (action)
    			action.cancel();		
    		//move to location (2, 0), not on virtual track
    		rpos::features::motion_planner::MoveOptions options;
    		options.flag = MoveOptionFlag(MoveOptionFlagMilestone | MoveOptionFlagPrecise);
    		action = sdp.moveTo(rpos::core::Location(2, 0), options);
    		action.waitUntilDone();
    		if (action.getStatus() == rpos::core::ActionStatusError)
    			std::cout << "Action Failed: " << action.getReason() << std::endl;
    		//draw a virtual track from (0, 0) to (2, 0), then move to (0, 0) via virtual track
    		rpos::core::Line line(rpos::core::Point(0,0),rpos::core::Point(2,0));
    		sdp.addLine(ArtifactUsageVirtualTrack, line);
    		options.flag = MoveOptionFlag(MoveOptionFlagKeyPoints | MoveOptionFlagPrecise);
    		action = sdp.moveTo(rpos::core::Location(0, 0), options);
    		action.waitUntilDone();
    		if (action.getStatus() == rpos::core::ActionStatusError)
    			std::cout << "Action Failed: " << action.getReason() << std::endl;
  • No labels