You are viewing an old version of this page. View the current version.

Compare with Current View Page History

« Previous Version 17 Next »

需要:

软件平台:

Visual Studio 2010 

Slamware Windows SDK: https://download.slamtec.com/api/download/slamware-sdk-windows/2.5.0%20dev%2020170718?lang=netural

RoboStudio(显示虚拟轨道和虚拟墙): https://download.slamtec.com/api/download/robostudio-installer-win32/1.1.0_rtm?lang=netural

Sample Code: 

硬件平台:

(以下任选其一)

Slamware SDP mini 

Slamware SDP

Slamware 套装 (基于Slamware导航方案的用户机器人系统)

Zeus/Apollo等底盘系统

编译运行:

      准备工作: 开启机器人系统电源,并用RoboStudio连上机器人.

Tips

RoboStudio的使用说明请参考: (TODO: 添加RoboStudio文档)

机器人如何连接请参考: (TODO: 连接文档)

  

  1. 在sample code所在文件夹中,打开samples Solution
  2. 右键artifacts_demo, 打开属性选项,将Slamware SDK 的include目录和lib目录添加到工程
  3. 右键artifacts_demo, 将此工程设置成StartUp project
  4. 点击F5运行

描述:

  1. 此sample为 windows console application, 需要在console中用命令行执行,用法为:artifacts_demo <IP address>  (注: 此IP地址为slamware模块的IP地址)

    或者在属性页面设置Command Arguments

  2.  可以同时连上RoboStudio来帮助显示虚拟墙/虚拟轨道(红色为虚拟墙,绿色为虚拟轨道)

  3. 代码功能说明: 删除所有虚拟墙/虚拟轨道、添加虚拟墙、添加虚拟轨道、移动虚拟墙(移动虚拟轨道用法类似)、删除指定虚拟轨道(删除指定虚拟墙用法类似)

    删除所有虚拟轨道/虚拟墙
    		SlamwareCorePlatform sdp = SlamwareCorePlatform::connect(argv[1], 1445);
            std::cout << "Clearing existing tracks and walls..." << std::endl;
    		sdp.clearLines(ArtifactUsageVirtualTrack);
    		sdp.clearLines(ArtifactUsageVirtualWall);
    添加虚拟墙
    		std::cout << "Adding virtual walls..." << std::endl;
    		std::vector<Line> walls;
    		//add a 8 * 8 virtual wall square
    		walls.push_back(Line(Point(-4, -4), Point(-4, 4)));
    		walls.push_back(Line(Point(-4, 4), Point(4, 4)));
    	    walls.push_back(Line(Point(4, 4), Point(4, -4)));
    		walls.push_back(Line(Point(4, -4), Point(-4, -4)));	
    		sdp.addLines(ArtifactUsageVirtualWall, walls);	
    添加虚拟轨道
    		std::cout << "Adding virtual tracks..." << std::endl;
    		std::vector<Line> tracks;
    		//add a 2 * 2 virtual track square
    		tracks.push_back(Line(Point(-1, -1), Point(-1, 1)));
    		tracks.push_back(Line(Point(-1, 1), Point(1, 1)));
    		tracks.push_back(Line(Point(1, 1), Point(1, -1)));
    		tracks.push_back(Line(Point(1, -1), Point(-1, -1)));	
    		sdp.addLines(ArtifactUsageVirtualTrack, tracks);
    移动虚拟墙
    		std::cout << "Moving vitual walls..." << std::endl;
    		//sleep 5 seconds for displaying purpose only, not necessary
    		boost::this_thread::sleep_for(boost::chrono::milliseconds(5000)); 
    		std::vector<Line> get_walls = sdp.getLines(ArtifactUsageVirtualWall);
    		//shrink virtual wall square from 8 * 8 to 6 *6
    		for (std::vector<Line>::iterator it = get_walls.begin() ; it != get_walls.end(); ++it) {			
    			it->startP().x() = it->startP().x() > 0 ?  --(it->startP().x()) : ++(it->startP().x()); 
    			it->startP().y() = it->startP().y() > 0 ?  --(it->startP().y()) : ++(it->startP().y());
    			it->endP().x() = it->endP().x() > 0 ?  --(it->endP().x()) : ++(it->endP().x()); 
    			it->endP().y() = it->endP().y() > 0 ?  --(it->endP().y()) : ++(it->endP().y());	
    		}
    		sdp.moveLines(ArtifactUsageVirtualWall, get_walls);
    删除指定虚拟轨道
    		std::cout << "Get all tracks..." << std::endl;
    		std::vector<Line> get_tracks = sdp.getLines(ArtifactUsageVirtualTrack);
    		for (std::vector<Line>::iterator it = get_tracks.begin() ; it != get_tracks.end(); ++it) {
    			std::cout << "ID: " << it->id() << std::endl;
    			std::cout << "Start from (" << it->startP().x() << " , " << it->startP().y() << ") " << "to (" 
    				      << it->endP().x() << " , " << it->endP().y() << " ) " << std::endl;		
    		}
    
    		std::cout << "Delete track by ID, please enter track ID:" << std::endl;
    		int id;
    	    bool is_found = false;
    		std::cin >> id ;
    		for (std::vector<Line>::iterator it = get_tracks.begin() ; it != get_tracks.end(); ++it) {
    			if (id == it->id()) {
    				sdp.removeLineById(ArtifactUsageVirtualTrack, id);
    				is_found = true;
    				break;
    			}
    		}
    		if(!is_found)
    			std::cout << "Wrong ID" << std::endl;

    4. Console 输出




  • No labels