You are viewing an old version of this page. View the current version.

Compare with Current View Page History

« Previous Version 4 Next »

需要:

Visual Studio 2010 

Slamware Windows SDK: https://download.slamtec.com/api/download/slamware-sdk-windows/2.5.0%20dev%2020170718?lang=netural

RoboStudio(显示虚拟轨道和虚拟墙): 

Sample Code: 

编译:

  1. 在sample code所在文件夹中,打开samples Solution
  2. 右键artifacts_demo, 打开属性选项,将Slamware SDK 的include目录和lib目录添加到工程
  3. 右键artifacts_demo, 将此工程设置成StartUp project
  4. 点击F5

描述:

  1. 此sample为 windows console application, 需要在console中用命令行执行,用法为:artifacts_demo <IP address>  (注: 此IP地址为slamware模块的IP地址)

    或者在属性页面设置Command Arguments
  2. 代码功能说明: 删除所有虚拟墙/虚拟轨道、添加虚拟墙、添加虚拟轨道、移动虚拟墙(移动虚拟轨道用法类似)、删除指定虚拟轨道(删除指定虚拟墙用法类似)

    删除所有虚拟轨道/虚拟墙
    		SlamwareCorePlatform sdp = SlamwareCorePlatform::connect(argv[1], 1445);
            std::cout << "Clearing existing tracks and walls..." << std::endl;
    		sdp.clearLines(ArtifactUsageVirtualTrack);
    		sdp.clearLines(ArtifactUsageVirtualWall);
    添加虚拟墙
    		std::cout << "Adding virtual walls..." << std::endl;
    		std::vector<Line> walls;
    		//add a 8 * 8 virtual wall square
    		walls.push_back(Line(Point(-4, -4), Point(-4, 4)));
    		walls.push_back(Line(Point(-4, 4), Point(4, 4)));
    	    walls.push_back(Line(Point(4, 4), Point(4, -4)));
    		walls.push_back(Line(Point(4, -4), Point(-4, -4)));	
    		sdp.addLines(ArtifactUsageVirtualWall, walls);	




  • No labels