Versions Compared

Key

  • This line was added.
  • This line was removed.
  • Formatting was changed.


Excerpt

本页介绍了get_power_status的用法, 包含当前的充电状态,电池电量等。




本页内容

Table of Contents


运行环境准备

  • 软件平台

    • Visual Studio 2010  SP1
    • Slamware Windows SDK:Slamware Windows SDK
    • RoboStudio(用于显示地图):Robostudio installer
    • Sample Code: 

      Info

      使用更高版本的Visual Studio可能会带来编译异常。

      使用Visual Studio 2010(无SP1)可能会因为无法与.Net Framework兼容而报编译错误,此时增加SP1更新包即可解决问题


  • 硬件平台

          (以下任选其一)

      • Slamware SDP mini 
      • Slamware SDP
      • Slamware 套装 (基于Slamware导航方案的用户机器人系统)
      • Zeus/Apollo等底盘系统


例程下载

Win32-例程下载


编译运行

  1. 打开samples工程,右键get_power_status, 将此工程设置成StartUp project


  2. 右键get_power_status, 打开属性选项,将Slamware SDK 的include目录和lib目录添加到工程

    Info

    Slamware SDK的include和lib目录无需复制到参考例程目录,只需在Visual Studio里指定路径即可。




  3. 右键get_power_status, 在Debugging页面中command Arguments处输入 192.168.11.1 
    格式说明:get_power_status <IP address> 


  4. 点击F5运行
  5. Console输出为


代码描述

  • 获取电量/充电状态

    Code Block
    languagecpp
    firstline1
    title获取电量/充电状态
    linenumberstrue
    		
            SlamwareCorePlatform sdp = SlamwareCorePlatform::connect(argv[1], 1445);
            std::cout <<"SDK Version: " << sdp.getSDKVersion() << std::endl;
            std::cout <<"SDP Version: " << sdp.getSDPVersion() << std::endl;
    		
    		PowerStatus status = sdp.getPowerStatus();
    		std::cout << "Battery Percentage: " << status.batteryPercentage << std::endl;
    		std::cout << "is Charging: " << status.isCharging << std::endl;
    		std::cout << "is DC connected: " << status.isDCConnected << std::endl;
    		
    		if(status.dockingStatus == DockingStatusNotOnDock)
    			std::cout << "Docking status: Not on dock" << std::endl;
    		else if(status.dockingStatus == DockingStatusOnDock)
    			std::cout << "Docking status: On dock" << std::endl;
    		else 
    			std::cout << "Docking status: Unknown" << std::endl;