Versions Compared

Key

  • This line was added.
  • This line was removed.
  • Formatting was changed.


Excerpt

本页介绍了move_to_spot的用法, 包含导航模式下和轨道模式下的运动到目标点的过程



本页内容

Table of Contents


运行环境准备

  • 软件平台

    • Visual Studio 2010  SP1
    • Slamware Windows SDK:Slamware Windows SDK
    • RoboStudio(用于显示地图):Robostudio installer
    • Sample Code: 

      Info

      使用更高版本的Visual Studio可能会带来编译异常。

      使用Visual Studio 2010(无SP1)可能会因为无法与.Net Framework兼容而报编译错误,此时增加SP1更新包即可解决问题


  • 硬件平台

          (以下任选其一)

      • Slamware SDP mini 
      • Slamware SDP
      • Slamware 套装 (基于Slamware导航方案的用户机器人系统)
      • Zeus/Apollo等底盘系统

例程下载

Win32-例程下载



编译运行

  1. 打开samples工程,右键move_to_spot, 将此工程设置成StartUp project
  2. 右键move_to_spot, 打开属性选项,将Slamware SDK 的include目录和lib目录添加到工程

    Info

    Slamware SDK的include和lib目录无需复制到参考例程目录,只需在Visual Studio里指定路径即可。


  3. 右键move_to_spot, 在Debugging页面中command Arguments处输入 192.168.11.1 
    格式说明: move_to_spot <IP address> 


  4. 点击F5运行
  5. 可以连上Robostudio查看地图及机器人的运动
    Multimedia
    namebandicam 2018-01-30 15-29-41-992.mp4


代码描述

  • 机器人导航运动到目标点(2, 0) ,期间遇到障碍物会自主避障,然后从(2,0) 沿虚拟轨道运动到目标点(0, 0)

    Code Block
    languagecpp
    firstline1
    title导航到目标点
    linenumberstrue
            SlamwareCorePlatform sdp = SlamwareCorePlatform::connect(argv[1], 1445);
    		std::cout <<"SDK Version: " << sdp.getSDKVersion() << std::endl;
    		std::cout <<"SDP Version: " << sdp.getSDPVersion() << std::endl;
    		rpos::actions::MoveAction action = sdp.getCurrentAction();
    		if (action)
    			action.cancel();		
    		//move to location (2, 0), not on virtual track
    		rpos::features::motion_planner::MoveOptions options;
    		options.flag = MoveOptionFlag(MoveOptionFlagMilestone | MoveOptionFlagPrecise);
    		action = sdp.moveTo(rpos::core::Location(2, 0), options);
    		action.waitUntilDone();
    		if (action.getStatus() == rpos::core::ActionStatusError)
    			std::cout << "Action Failed: " << action.getReason() << std::endl;
    		//draw a virtual track from (0, 0) to (2, 0), then move to (0, 0) via virtual track
    		rpos::core::Line line(rpos::core::Point(0,0),rpos::core::Point(2,0));
    		sdp.addLine(ArtifactUsageVirtualTrack, line);
    		options.flag = MoveOptionFlag(MoveOptionFlagKeyPoints | MoveOptionFlagPrecise);
    		action = sdp.moveTo(rpos::core::Location(0, 0), options);
    		action.waitUntilDone();
    		if (action.getStatus() == rpos::core::ActionStatusError)
    			std::cout << "Action Failed: " << action.getReason() << std::endl;