Versions Compared

Key

  • This line was added.
  • This line was removed.
  • Formatting was changed.


Excerpt

本页介绍了composite_map_demo的用法, 主要包含对.stcm地图格式的composite

map的读写操作

map的读写操作。



本页内容

Table of Contents
stylesquare


运行环境准备

  • 软件平台

    • Visual Studio 2010  SP1
    • Slamware Windows SDK:Slamware Windows SDK
    • RoboStudio(用于显示地图):Robostudio installer 
    • Sample Code: 

      Info

      使用更高版本的Visual Studio可能会带来编译异常。

      使用Visual Studio 2010(无SP1)可能会因为无法与.Net Framework兼容而报编译错误,此时增加SP1更新包即可解决问题


  • 硬件平台

          (以下任选其一)

    • Slamware SDP mini 
    • Slamware SDP
    • Slamware 套装 (基于Slamware导航方案的用户机器人系统)
    • Zeus/Apollo等底盘系统


编译运行

例程下载

打开samples工程

Win32-例程下载



Image Removed

编译运行

  1. 打开samples工程,右键composite_map_demo,

    打开属性选项,将Slamware SDK 的include目录和lib目录添加到工程

    将此工程设置成StartUp project

    Image Added


    Image Removed

  2. 右键composite_map_demo,

    将此工程设置成StartUp project

    打开属性选项,将Slamware SDK 的include目录和lib目录添加到工程


    Info

    Slamware SDK的include和lib目录无需复制到参考例程目录,只需在Visual Studio里指定路径即可。


    Image Added

  3. 右键composite_map_demo, 打开properties选项,设置Command Arguments 如下图,

    格式说明:

    composite_map_demo  [OPTS]

     

    [filename]

     

    <SDP IP Address>
    SDP IP Address           

     The

    The ip address string of the SLAMWARE SDP
    getstcm filename         

    download compositeMap
                                         If not specified, the default name map.stms will be used

     download compositeMap
    setstcm filename         

    upload

     upload compositeMap
    -h                                 

    Show

     Show this message

  4. 点击F5运行

    • composite_map_demo getstcm map.stcm 192.168.11.1 (从slamware里面读取composite map, 并生成map.stcm)

      可以用Robostudio的地图编辑器来查看生成的地图:
    • composite_map_demo setstcm map.stcm 192.168.11.1(将名为map.stcm的地图上传至slamware)

      可以在Robostudio中连上机器人,可以看到地图已经上传成功


代码描述

  • 从slamware模块下载composite map到客户端
Code Block
languagecpp
firstline1
title获取composite map
linenumberstrue
bool StcmMapWriter(const std::string file_name, SlamwareCorePlatform platform) {
	CompositeMap composite_map = platform.getCompositeMap();
    CompositeMapWriter composite_map_writer;
    std::string error_message;
    bool result = composite_map_writer.saveFile(error_message, file_name, composite_map);
    return result;
}


  •  从客户端上传composite map至slamware模块
Code Block
languagecpp
firstline1
title设置composite map
linenumberstrue
bool StcmMapReader(const std::string file_path, rpos::core::Pose pose, SlamwareCorePlatform platform) {
    CompositeMapReader composite_map_reader;
    std::string error_message;
    boost::shared_ptr<CompositeMap> composite_map(composite_map_reader.loadFile(error_message, file_path));
    if (composite_map) {
        platform.setCompositeMap((*composite_map), pose);	
        return true;
    }
    return false;
}


  • 从composite map中读取虚拟轨道,虚拟墙等信息
Code Block
languagecpp
firstline1
title读取map layer信息
linenumberstrue
    CompositeMapReader composite_map_reader;
    std::string error_message;
    boost::shared_ptr<CompositeMap> composite_map(composite_map_reader.loadFile(error_message, file_path));
    if (composite_map) {
        for (auto it = composite_map->maps().begin(); it != composite_map->maps().end(); ++it) {
            auto layer = *it;
            std::string usage = layer->getUsage();
			std::string type = layer->getType();
			std::cout << "Layer Usage : " << usage << std::endl;
			//get grid map layer
            if (type == GridMapLayer::Type) {
				auto grid_map = boost::dynamic_pointer_cast<GridMapLayer>(layer);
				std::cout << "Map Position : (" << grid_map->getOrigin().x() << " , " << 
					grid_map->getOrigin().y() << ")" <<std::endl;
				std::cout << "Map Resolution : (" << grid_map->getResolution().x() <<  
					" , " << grid_map->getResolution().y() << ")" <<std::endl;
				std::cout << "Map Dimension: (" << grid_map->getDimension().x() << 
					" , " << grid_map->getDimension().y() << ")" <<std::endl;
				std::cout << "Map Data:" << std::endl;
				for (auto it = grid_map->mapData().begin(); it != grid_map->mapData().end(); ++it) {
					std::cout << (int)*it << " " ;				
				}
				std::cout << std::endl << std::endl;			
            }
			//get line map layer
            else if (type == LineMapLayer::Type) {
                auto line_map = boost::dynamic_pointer_cast<LineMapLayer>(layer);
				for (auto it = line_map->lines().begin(); it != line_map->lines().end(); ++it) {
					auto line = it->second;
					std::cout << "start: (" << line.start.x() << " , " << line.start.y() << ")" << std::endl;
					std::cout << "end: (" << line.end.x() << " , " << line.end.y() << ")" << std::endl;
				}
				std::cout << std::endl;
            }
			//get pose map layer
			else if (type == PoseMapLayer::Type) {
				auto pose_map = boost::dynamic_pointer_cast<PoseMapLayer>(layer);
				for (auto it = pose_map->poses().begin(); it != pose_map->poses().end(); ++it) {					
					auto pos = it->second;
					std::cout << "Position : (" << pos.pose.x() << " , " << pos.pose.y() << ")" << std::endl;
				}	
				std::cout << std::endl;
			}
			else if (type == PointsMapLayer::Type) {                
				//TODO: get Points map layer
				std::cout << std::endl;
            }
			else {
				//TODO: get unknown map layer
				std::cout << std::endl;
            }
        }