Versions Compared

Key

  • This line was added.
  • This line was removed.
  • Formatting was changed.

...

Table of Contents
maxLevel2
outlinetrue
absoluteUrltrue
stylecircle


Anchor
Go back to the Contents
Go back to the Contents


...

用法简介

格式

Code Block
languagecpp
firstline0
linenumberstrue
slamware_console base [options] <command> [cmd_arguments]

可用选项

选项名称

简写

描述

备注

--channel

-c channel

The communication channel with the base, supported channels: serial, tcp

 

--help

-h help

Show this message

 

--port

-p port

Trace communication between host and base

 

--trace-comm

-t trace comm

Trace communication between host and base

 

--version

-v print version number

Print version number

 

--host

host

The host used to communicate with the base (required for tcp channel)

 

命令概览

命令名称

描述

备注

beacon

Read auto home IR beacon data

 

bumper

Read bumper, cliff sensor data

 

config

Read configuration from base

 

event

Send Event Cmd

 

monitor

Continiously read sensor data and output to the console

 

motor

Read motor information, such as wheels' odometry

 

poll

Poll Base Cmd

 

run

Make motor run

 

sensor

Read distance sensors' data, such as ultrasonic data

 

status

Read base status, such as battery, charging status and etc.

 

test

Test base control bus protocol

 

vrun

Vector run. vrun <vx> <vy> <omega> <time>. Units: m/s m/s rad/s s

 

SA001 Slamware Console Application Note



命令用法及代码示例


Info
如下所有代码示例使用的接口假设为COM3

BEACON

读取自动返回充电时红外灯塔数据。

代码示例

Code Block
firstline0
titleslamware_console.exe base -c serial -p COM3 beacon
linenumberstrue
collapsetrue
C:\Users\LW\Desktop\tools\slamware_console_tool>slamware_console.exe base -c serial -p COM3 beacon
[rp.slamware.test.SlamwareConsoleApplication][INFO] Slamware Console 1.7.0
[rp.slamware.utils.ChannelFactory] [INFO]Connecting to serial:COM3...
[rp.slamware.test.SlamwareBaseConsoleApplication][INFO] Connected to Control Bus Device at serial:COM3
[rp.slamware.test.SlamwareBaseConsoleApplication][INFO] Model: ref base
[rp.slamware.test.SlamwareBaseConsoleApplication][INFO] Firmware Version: 1.83
[rp.slamware.test.SlamwareBaseConsoleApplication][INFO] Hardware version: 0.1
[rp.slamware.test.SlamwareBaseConsoleApplication][INFO] Serial Number: C47DDDC6F19575BD90AB43C0
[rp.slamware.test.SlamwareBaseConsoleApplication][INFO] Found 3 beacons and 3 probes
[rp.slamware.test.SlamwareBaseConsoleApplication][INFO]   Probe #0: 0:     1:    2:     
[rp.slamware.test.SlamwareBaseConsoleApplication][INFO]   Probe #1: 0:     1:    2:     
[rp.slamware.test.SlamwareBaseConsoleApplication][INFO]   Probe #2: 0:     1:    2:     
[rp.slamware.test.SlamwareConsoleApplication][INFO] Successfully executed command

BUMPER

...