Versions Compared

Key

  • This line was added.
  • This line was removed.
  • Formatting was changed.

...

  1. 右键composite_map_demo, 打开属性选项,将Slamware SDK 的include目录和lib目录添加到工程
  2. 右键composite_map_demo, 将此工程设置成StartUp project
  3. 点击F5 运行
  4. 在debug目录下用命令行运行composite_map_demo, 用法如下:

    composite_map_demo  [OPTS]  [filename]  <SDP IP Address>
    SDP IP Address           The ip address string of the SLAMWARE SDP
    getstcm filename          download compositeMap
                                         If not specified, the default name map.stms will be used
    setstcm filename          upload compositeMap
    -h                                  Show this message

  5. 从slamware里面读取composite map(此操作会在桌面上生成一个test.stcm的地图文件,并在console中输出地图数据信息):
    Image Modified
    可以用Robostudio的地图编辑器来查看生成的地图:

  6. 将本地的composite map上传至slamware
    可以先在Robostudio里面查看将要上传的地图:

    将此底图上传至slamware:
    Image RemovedImage Added
    可以在Robostudio中连上机器人,可以看到地图已经上传成功


...