This page introduces the usage of sync_set_stcm, including how to upload the STCM map to the robot via the sync_set_stcm service.
Contents
Environment Setup
software platform
- Ubuntu 20.04 X86
- ROS Noetic
hardware platform
Choose any one below:
- Slamware Kit (User Robot System based on Slamware Solution)
- robot base systems like Apollo/Ares/Athena
Sample Code Download
Compile and Run
- Download the Slamware ROS SDK along with ROS examples.
- Place the 'src' folder from the ROS SDK into an empty working directory, such as 'catkin_ws'. Also, put the 'slamware_ros_sample' folder from the ROS examples into the 'src' folder.
mkdir -p catkin_ws/src cd catkin_ws/src
- Initialize the workspace using the Catkin tool.
catkin_init_workspace
- Compile.
cd .. catkin_make
- Set up workspace environment.
source devel/setup.bash
- Launch the slamware_ros_sdk_server_node node. Select the corresponding IP according to the mode.
roslaunch slamware_ros_sdk slamware_ros_sdk_server_node.launch ip_address:=10.6.128.141 // Station mode // If in AP mode, the IP address is 192.168.11.1
- Open another terminal, repeat step 5, and start the sync_set_stcm_node node.
roslaunch slamware_ros_sample sync_set_stcm.launch // In the launch file, there is a default definition for the map_file_name parameter, indicating the path and filename where the map is saved. you can adjust parameters manually.
- At this point, observe the RVIZ interface; if the map file is successfully located, the map will be uploaded, and the map in RVIZ will also change accordingly. Otherwise, an error will occur.
Code Description
sync_set_stcm
int main (int argc, char **argv)
{
std::string map_file_name;
long data_size;
ros::init(argc, argv, "sync_set_stcm_node");
ros::NodeHandle nh("~");
ros::ServiceClient client = nh.serviceClient<slamware_ros_sdk::SyncSetStcm>("/slamware_ros_sdk_server_node/sync_set_stcm");
slamware_ros_sdk::SyncSetStcm srv;
//get file name from paramter server
if (!nh.getParam("map_file_name",map_file_name))
{
ROS_ERROR("invalied file path......");
return 1;
}
ROS_INFO("map file path: %s",map_file_name.c_str());
//open map file and get data
std::ifstream fin(map_file_name ,std::ios::in | std::ios::binary | std::ios::ate);
if(!fin.is_open())
{
ROS_ERROR("open map file failed......");
return 1;
}
ROS_INFO("open map file success,reading data......");
data_size = fin.tellg();
fin.seekg(0,std::ios::beg);
srv.request.raw_stcm.resize(data_size);
fin.read(reinterpret_cast<char *>(srv.request.raw_stcm.data()),data_size*sizeof(srv.request.raw_stcm.front()));
fin.close();
ROS_INFO("raw_stcm data size: %zu",srv.request.raw_stcm.size());
//set robot pose
srv.request.robot_pose.position.x = 0;
srv.request.robot_pose.position.y = 0;
srv.request.robot_pose.position.z = 0;
srv.request.robot_pose.orientation.x = 0;
srv.request.robot_pose.orientation.y = 0;
srv.request.robot_pose.orientation.z = 0;
srv.request.robot_pose.orientation.w = 1;
//call service
if (client.call(srv))
{
ROS_INFO("set stcm map success......");
}
else
{
ROS_ERROR("Failed to set stcm map......");
return 1;
}
return 0;
}