The page introduces the usage of teleop_twist_keyboard, including how to control the motion of a robot using the keyboard.
Contents
Environment Setup
software platform
- Ubuntu 20.04 X86
- ROS Noetic
hardware platform
Choose any one below:
- Slamware Kit (User Robot System based on Slamware Solution)
- robot base systems like Apollo/Ares/Athena
Sample Code Download
Compile and Run
- Download the Slamware ROS SDK along with ROS examples.
- Place the 'src' folder from the ROS SDK into an empty working directory, such as 'catkin_ws'. Also, put the 'slamware_ros_sample' folder from the ROS examples into the 'src' folder.
mkdir -p catkin_ws/src cd catkin_ws/src
- Initialize the workspace using the Catkin tool.
catkin_init_workspace
- Compile.
cd .. catkin_make
- Set up workspace environment.
source devel/setup.bash
- Launch the slamware_ros_sdk_server_node node. Select the corresponding IP according to the mode.
roslaunch slamware_ros_sdk slamware_ros_sdk_server_node.launch ip_address:=10.6.128.141 // Station mode // If in AP mode, the IP address is 192.168.11.1
- Open another terminal, repeat step 5, and start the teleop_twist_keyboard_node node. Follow the prompts and use the W/S/A/D keys to control the robot to move forward/backward/left/right accordingly.
roslaunch slamware_ros_sample teleop_twist_keyboard.launch
Code Description
Define keyboard buttons
moveBindings = {
'w':(1.0, 0.0),
's':(-1.0, 0.0),
'a':(0.0, 1.0),
'd':(0.0, -1.0)
}
Define a publisher, specify the topic name and type
pub = rospy.Publisher('/cmd_vel', Twist, queue_size = 1)
Initialize node
rospy.init_node('teleop_twist_keyboard_node')
When pressing keys, assign the velocity to linearX and angularZ
key = getKey()
print(key)
if key in moveBindings.keys():
linearX = moveBindings[key][0]
angularZ = moveBindings[key][1]
else:
linearX = 0.0
angularZ = 0.0
if (key == '\x03'):
break
Publish messages according to the required type of topic
twist = Twist() twist.linear.x = linearX twist.angular.z = angularZ pub.publish(twist)