This page introduces the usage of display_virtual_lines, including how to display virtual walls in rviz.
Contents
Environment Setup
software platform
- Ubuntu 20.04 X86
- ROS Noetic
hardware platform
Choose any one below:
- Slamware Kit (User Robot System based on Slamware Solution)
- robot base systems like Apollo/Ares/Athena
Sample Code Download
Compile and Run
- Download the Slamware ROS SDK along with ROS examples.
- Place the 'src' folder from the ROS SDK into an empty working directory, such as 'catkin_ws'. Also, put the 'slamware_ros_sample' folder from the ROS examples into the 'src' folder.
mkdir -p catkin_ws/src cd catkin_ws/src
- Initialize the workspace using the Catkin tool.
catkin_init_workspace
- Compile.
cd .. catkin_make
- Set up workspace environment.
source devel/setup.bash
- Launch the slamware_ros_sdk_server_node node. Select the corresponding IP according to the mode.
roslaunch slamware_ros_sdk slamware_ros_sdk_server_node.launch ip_address:=10.6.128.141 // Station mode // If in AP mode, the IP address is 192.168.11.1
- Open another terminal, repeat step 5, and start the view_slamware_ros_sdk_server_node node.
roslaunch slamware_ros_sdk view_slamware_ros_sdk_server_node.launch
- Open another terminal, repeat step 5, and start the display_virtual_lines_node node.
roslaunch slamware_ros_sample display_virtual_lines.launch
- Configure and add the display of Marker information in Rviz:
Click 'Add' in the bottom-left corner of Rviz, then in the pop-up window, select 'Marker' and click 'OK'. Upon success, as shown in the image below, a Marker is added to Displays, and the virtual walls are also displayed in the interface.
Code Description
Initialize the node, define publisher and subscriber objects
ros::init(argc, argv, "display_virtual_lines_node"); ros::NodeHandle n; ros::Publisher pub = n.advertise<visualization_msgs::Marker>("visualization_marker", 10); ros::Subscriber sub = n.subscribe<slamware_ros_sdk::Line2DFlt32Array>("/slamware_ros_sdk_server_node/virtual_walls", 30, virtualWallCallback);
Declare a global variable of type Marker named "lines" to store the published virtual walls
visualization_msgs::Marker lines;
Upon receiving the virtual wall message sent by the slamware_ros_sdk_server_node, save it into the "lines" variable
void virtualWallCallback(const slamware_ros_sdk::Line2DFlt32Array::ConstPtr & msg) { lines.points.clear(); size_t cnt = msg->lines.size(); for (size_t i = 0; i < msg->lines.size(); ++i) { geometry_msgs::Point p1; p1.x = msg->lines[i].start.x; p1.y = msg->lines[i].start.y; p1.z = 0.2; geometry_msgs::Point p2; p2.x = msg->lines[i].end.x; p2.y = msg->lines[i].end.y; p2.z = 0.2; lines.points.push_back(p1); lines.points.push_back(p2); } }
Configure "lines", such as type, size, color, etc
lines.id = 1; lines.header.frame_id = "slamware_map"; lines.type = visualization_msgs::Marker::LINE_LIST; lines.ns = "lines"; lines.action = visualization_msgs::Marker::ADD; lines.pose.orientation.w = 1.0; lines.scale.x = 0.1; lines.color.r = 1.0; lines.color.a = 1.0;
Publish "lines"
ros::Rate r(30); while(running) { lines.header.stamp = ros::Time::now(); pub.publish(lines); r.sleep(); }