本页介绍了sync_get_stcm的用法, 包含如何通过sync_get_stcm服务获取stcm地图。 |
本页内容
(以下任选其一)
1.下载Slamware ROS SDK以及ROS例程。
2.将ROS sdk中的src文件夹放入一个空的工作目录,如:catkin_ws。将ROS 例程中的slamware_ros_sample文件夹也放入src文件夹下。使用catkin工具初始化工作空间。
cd catkin_ws/src catkin_init_workspace |
3.编译
cd .. catkin_make |
4.配置工作空间系统环境
source devel/setup.bash |
5.启动slamware_ros_sdk_server_node节点
roslaunch slamware_ros_sdk slamware_ros_sdk_server_node.launch ip_address:=10.6.128.141 //如果是AP模式,ip_address是192.168.11.1 |
6.重新打开一个终端窗口,重复第4步,并启动sync_get_stcm_node节点
roslaunch slamware_ros_sample sync_get_stcm.launch //launch文件中有定义默认的map_file_name参数,指明地图保存的路径和文件名称。如果不用默认参数,可自行传参。 |
7.此时观察slamware_ros_sample下,会生成一个map的文件夹,里面会生成data.map的文件。
int main (int argc, char **argv) { std::string map_file_name; ros::init(argc, argv, "sync_set_stcm_node"); ros::NodeHandle nh("~"); ros::ServiceClient client = nh.serviceClient<slamware_ros_sdk::SyncGetStcm>("/slamware_ros_sdk_server_node/sync_get_stcm"); slamware_ros_sdk::SyncGetStcm srv; //get file name from paramter server if (!nh.getParam("map_file_name",map_file_name)) { ROS_ERROR("invalied file path......"); return 1; } //call service if (client.call(srv)) { ROS_INFO("get raw_stcm data success,writing to file......"); //check whether the target folder exists. create one if not std::string dir; dir = map_file_name.substr(0,map_file_name.rfind("/")); if(access(dir.c_str(),0)) { std::string cmd = "mkdir -p " + dir; system(cmd.c_str()); } std::ofstream fout(map_file_name, std::ios::out | std::ios::binary); fout.write(reinterpret_cast<char *>(srv.response.raw_stcm.data()),(srv.response.raw_stcm.size()) * sizeof(srv.response.raw_stcm.front())); fout.close(); ROS_INFO("raw_stcm data size: %zu",srv.response.raw_stcm.size()); ROS_INFO("save map at %s success......",map_file_name.c_str()); } else { ROS_ERROR("Failed to get raw_stcm data......"); return 1; } return 0; } |