本页介绍了move_to_spot的用法, 包含导航模式下和轨道模式下的运动到目标点的过程。 |
本页内容
Sample Code:
使用更高版本的Visual Studio可能会带来编译异常。 使用Visual Studio 2010(无SP1)可能会因为无法与.Net Framework兼容而报编译错误,此时增加SP1更新包即可解决问题 |
(以下任选其一)
右键move_to_spot, 打开属性选项,将Slamware SDK 的include目录和lib目录添加到工程
Slamware SDK的include和lib目录无需复制到参考例程目录,只需在Visual Studio里指定路径即可。 |
机器人导航运动到目标点(2, 0) ,期间遇到障碍物会自主避障,然后从(2,0) 沿虚拟轨道运动到目标点(0, 0)
SlamwareCorePlatform sdp = SlamwareCorePlatform::connect(ip_address, 1445); std::cout <<"SDK Version: " << sdp.getSDKVersion() << std::endl; std::cout <<"SDP Version: " << sdp.getSDPVersion() << std::endl; while(true){ BaseHealthInfo robot_health = sdp.getRobotHealth(); if(robot_health.hasError) std::cout << "Error" << std::endl; if(robot_health.hasFatal) std::cout << "Fatal" << std::endl; if(robot_health.hasWarning) std::cout << "Warning" << std::endl; if(*robot_health.hasLidarDisconnected) std::cout << "LidarDisconnected" << std::endl; if(*robot_health.hasSdpDisconnected) std::cout << "SdpDisconnected" << std::endl; if(*robot_health.hasSystemEmergencyStop) std::cout << "SystemEmergencyStop" << std::endl; for (auto it = robot_health.errors.begin();it != robot_health.errors.end(); ++ it) { std::cout << "Message: " << it->message << std::endl; std::cout << "Level: " << it->level << std::endl; std::cout << "ErrorType: "<< it->componentErrorType <<std::endl; std::cout << "ErrorCode: " << it->errorCode << std::endl; } int errors_size = robot_health.errors.size(); if(errors_size > 0){ std::cout << "Press 'y' to clear errors, press any other key to continue..." << std::endl; char is_error_clear; std::cin >> is_error_clear; if(is_error_clear == 'y' || is_error_clear == 'Y') { for (auto it = robot_health.errors.begin();it != robot_health.errors.end(); ++ it) { sdp.clearRobotHealth(it->errorCode); std::cout << "Error: " << it->message << " cleared!" << std::endl; } } } } |