软件平台:
硬件平台:
(以下任选其一)
configure_network_demo [OPTS] <SDP IP Address>
slamware_address The ip address string of the SLAMWARE SDP.
AP Configurate network in AP mode.
STA Configurate network in STA mode.
--disable-dhcp disable dhcp.
--enable-dhcp enable dhcp.
--disable-wifi disable wifi
-h Show this message
同样,可以disable/enable DHCP, disable WIFI, 使用命令如上所述,在此不具体描述。
代码功能说明:将slamware模块配置成AP模式, 将slamware模块配置成STA模式, 关闭/打开DHCP, 关闭WIFI 等
std::map<std::string, std::string> options; options["ssid"] = "test"; options["password"] = "12345678"; // password length should surpass 8 options["ip"] = "192.168.11.101"; // do not use address from 192.168.11.1 to 192.168.11.100 (reserved for internal usage) options["channel"] = "6"; result = sdp.configurateNetwork(NetworkMode::NetworkModeAP, options); |
std::map<std::string, std::string> options; options["ssid"] = ssid; options["password"] = password; result = sdp.configurateNetwork(NetworkMode::NetworkModeStation, options); |