This page introduces the usage of sync_get_stcm, including how to retrieve the STCM map through the sync_get_stcm service.
Contents
Environment Setup
software platform
- Ubuntu 20.04 X86
- ROS Noetic
hardware platform
Choose any one below:
- Slamware Kit (User Robot System based on Slamware Solution)
- robot base systems like Apollo/Ares/Athena
Sample Code Download
Compile and Run
- Download the Slamware ROS SDK along with ROS examples.
- Place the 'src' folder from the ROS SDK into an empty working directory, such as 'catkin_ws'. Also, put the 'slamware_ros_sample' folder from the ROS examples into the 'src' folder.
mkdir -p catkin_ws/src cd catkin_ws/src
- Initialize the workspace using the Catkin tool.
catkin_init_workspace
- Compile.
cd .. catkin_make
- Set up workspace environment.
source devel/setup.bash
- Launch the slamware_ros_sdk_server_node node. Select the corresponding IP according to the mode.
roslaunch slamware_ros_sdk slamware_ros_sdk_server_node.launch ip_address:=10.6.128.141 // Station mode // If in AP mode, the IP address is 192.168.11.1
- Open another terminal, repeat step 5, and start the sync_get_stcm_node node.
roslaunch slamware_ros_sample sync_get_stcm.launch // In the launch file, there is a default definition for the map_file_name parameter, indicating the path and filename where the map is saved. you can adjust parameters manually.
- At this point, observe under slamware_ros_sample, a folder named 'map' will be generated, containing a file named 'data.map'.
Code Description
sync_get_stcm
int main (int argc, char **argv) { std::string map_file_name; ros::init(argc, argv, "sync_set_stcm_node"); ros::NodeHandle nh("~"); ros::ServiceClient client = nh.serviceClient<slamware_ros_sdk::SyncGetStcm>("/slamware_ros_sdk_server_node/sync_get_stcm"); slamware_ros_sdk::SyncGetStcm srv; //get file name from paramter server if (!nh.getParam("map_file_name",map_file_name)) { ROS_ERROR("invalied file path......"); return 1; } //call service if (client.call(srv)) { ROS_INFO("get raw_stcm data success,writing to file......"); //check whether the target folder exists. create one if not std::string dir; dir = map_file_name.substr(0,map_file_name.rfind("/")); if(access(dir.c_str(),0)) { std::string cmd = "mkdir -p " + dir; system(cmd.c_str()); } std::ofstream fout(map_file_name, std::ios::out | std::ios::binary); fout.write(reinterpret_cast<char *>(srv.response.raw_stcm.data()),(srv.response.raw_stcm.size()) * sizeof(srv.response.raw_stcm.front())); fout.close(); ROS_INFO("raw_stcm data size: %zu",srv.response.raw_stcm.size()); ROS_INFO("save map at %s success......",map_file_name.c_str()); } else { ROS_ERROR("Failed to get raw_stcm data......"); return 1; } return 0; }