Versions Compared

Key

  • This line was added.
  • This line was removed.
  • Formatting was changed.

...

11.What are the functions of the two switches next to the system switch?

Name

Image

Description

Remarks

Emergency stop switch

Image Modified

It is used during emergency situations. When switch is pressed, the device will stop immediately.



Brake release switch

Image Modified

Pressing this switch after the device has been turned on will release the brake and allow you to push around freely; pressing it again will reapply the brake and prevent you from pushing the device freely.

When the device is not powered on, this brake switch is invalid.

12.How to build a map?

Turn on the device, establish a connection with it using RoboStudio, then move the device using the controls. Once the entire map is constructed, you can modify it by adding POI points and other map components.

...

It can be modified. Food Delivery App has a function for speed modification, which can be operated directly through the screen, and the modification range is 0.2m/s~0.7m1m/s~1,0m/s. (If you need to increase the speed, commercial customization is available.)

...

25.What is the meaning of charging stationindicator status?

Process

Prefabricated condition

Indicator light status

Description

Power on and power off

charging station power on

Red light always on

Indicates that the charging station is properly powered up

charging station power off

Red light off

Indicates that the charging station is disconnected from power

Automatic charging

The charging station is charging the main unit

Green light flash slowly (breathing flash)

Indicates that the device is charging at the charging station

The device is fully charged

Green Light  Always on

Indicates that the device is fully charged

Abnormal Status

charging station power-up self-test abnormal

Red light flashing quickly

Abnormal collision, check whether the charging shrapnel is normal

charging station fuse anomaly

Red light flashing slowly

Self-restoring fuse popped, need to press to restore

charging station working abnormally

Alternating red and green light flash slowly

charging station abnormal or device abnormal (when there is no contact between device and charging station, it means charging station abnormal)

26.Is there any requirement for the location of charging station?

...