Versions Compared

Key

  • This line was added.
  • This line was removed.
  • Formatting was changed.
Excerpt

本页介绍了display_virtual_lines的用法, 包含如何在rviz中显示虚拟墙的功能。

本页内容

Table of Contents


运行环境准备

  • 软件平台

    • Ubuntu 16.04 AMD04 X86
    • ROS Kinetic
  • 硬件平台

          (以下任选其一)

      • Slamware 套装 (基于Slamware导航方案的用户机器人系统)
      • Apollo/Ares/Athena等底盘系统

例程下载

ROS-例程下载


编译运行

1.下载Slamware ROS SDK以及ROS例程。

2.将ROS sdk中的src文件夹放入一个空的工作目录,如:catkin_ws。将ROS 例程中的slamware_ros_sample文件夹也放入src文件夹下。使用catkin工具初始化工作空间。

Code Block
cd catkin_ws/src
catkin_init_workspace

3.编译

Code Block
cd ..
catkin_make

4.配置工作空间系统环境

Code Block
source devel/setup.bash

5.启动slamware_ros_sdk_server_node节点

Code Block
roslaunch slamware_ros_sdk slamware_ros_sdk_server_node.launch ip_address:=10.6.128.141
//如果是AP模式,ip_address是192.168.11.1

6.重新打开一个终端窗口,重复第4步,并启动view_slamware_ros_sdk_server_node节点

Code Block
roslaunch slamware_ros_sdk view_slamware_ros_sdk_server_node.launch

7.重新打开一个终端窗口,重复第4步,并启动display_virtual_lines_node节点

Code Block
roslaunch slamware_ros_sample display_virtual_lines.launch

8.在Rviz中配置添加显示Marker信息。点击Rviz左下角的Add,在弹出的窗口中,选择Marker,点击OK。成功后,会如下图,在Displays加入了一个Marker,虚拟墙也在界面中显示


代码描述


Code Block
languagecpp
firstline1
title初始化节点,定义publisher和subcriber对象
ros::init(argc, argv, "display_virtual_lines_node");
ros::NodeHandle n;
ros::Publisher pub = n.advertise<visualization_msgs::Marker>("visualization_marker", 10);
ros::Subscriber sub = n.subscribe<slamware_ros_sdk::Line2DFlt32Array>("/slamware_ros_sdk_server_node/virtual_walls", 30, virtualWallCallback);
Code Block
languagecpp
title声明一个全局的Maker类型变量lines,用以存储发布的虚拟墙
visualization_msgs::Marker lines;
Code Block
languagecpp
title接收到slamware_ros_sdk_server_node节点发来的虚拟墙消息后,保存到lines中
void virtualWallCallback(const slamware_ros_sdk::Line2DFlt32Array::ConstPtr & msg)
{
    lines.points.clear();
    size_t cnt = msg->lines.size();
    for (size_t i = 0; i < msg->lines.size(); ++i)
    {
        geometry_msgs::Point p1;
        p1.x = msg->lines[i].start.x;
        p1.y = msg->lines[i].start.y;
        p1.z = 0.2;

        geometry_msgs::Point p2;
        p2.x = msg->lines[i].end.x;
        p2.y = msg->lines[i].end.y;
        p2.z = 0.2;

        lines.points.push_back(p1);
        lines.points.push_back(p2);
    }
}
Code Block
languagecpp
title配置lines,如:类型、尺寸、颜色等
lines.id = 1;
lines.header.frame_id = "slamware_map";
lines.type = visualization_msgs::Marker::LINE_LIST;
lines.ns = "lines";
lines.action = visualization_msgs::Marker::ADD;
lines.pose.orientation.w = 1.0;

lines.scale.x = 0.1;
lines.color.r = 1.0;
lines.color.a = 1.0;
Code Block
languagecpp
title将lines发布出去
ros::Rate r(30);
while(running)
    {
        lines.header.stamp = ros::Time::now();
        pub.publish(lines);

        r.sleep();
    }