The page introduces the usage of teleop_twist_keyboard, including how to control the motion of a robot using the keyboard.
...
Contents
Table of Contents | ||
---|---|---|
|
...
Environment Setup
software platform
...
- Slamware Kit (User Robot System based on Slamware Solution)
- robot base systems like Apollo/Ares/Athena
...
Sample Code Download
...
Compile and Run
- Download the Slamware ROS SDK along with ROS examples.
- Place the 'src' folder from the ROS SDK into an empty working directory, such as 'catkin_ws'. Also, put the 'slamware_ros_sample' folder from the ROS examples into the 'src' folder.
Code Block language bash mkdir -p catkin_ws/src cd catkin_ws/src
- Initialize the workspace using the Catkin tool.
Code Block language bash catkin_init_workspace
- Compile.
Code Block language bash cd .. catkin_make
- Set up workspace environment.
Code Block language bash source devel/setup.bash
- Launch the slamware_ros_sdk_server_node node. Select the corresponding IP according to the mode.
Code Block language bashcpp roslaunch slamware_ros_sdk slamware_ros_sdk_server_node.launch ip_address:=10.6.128.141 // Station mode // If in AP mode, the IP address is 192.168.11.1
- Open another terminal, repeat step 5, and start the teleop_twist_keyboard_node node. Follow the prompts and use the W/S/A/D keys to control the robot to move forward/backward/left/right accordingly.
Code Block language bash roslaunch slamware_ros_sample teleop_twist_keyboard.launch
...
Code Description
Code Block | ||||
---|---|---|---|---|
| ||||
moveBindings = { 'w':(1.0, 0.0), 's':(-1.0, 0.0), 'a':(0.0, 1.0), 'd':(0.0, -1.0) } |
...