This page introduces the usage of sync_get_stcm, including how to retrieve the STCM map through the sync_get_stcm service.
Environment Setup
- Ubuntu 20.04 X86
- ROS Noetic
Choose any one below:
- Slamware Kit (User Robot System based on Slamware Solution)
- robot base systems like Apollo/Ares/Athena
Sample Code Download
ROS-Sample Download Link
Compile and Run
- Download the Slamware ROS SDK along with ROS examples.
- Place the 'src' folder from the ROS SDK into an empty working directory, such as 'catkin_ws'. Also, put the 'slamware_ros_sample' folder from the ROS examples into the 'src' folder.
Code Block |
---|
|
mkdir -p catkin_ws/src
cd catkin_ws/src |
- Initialize the workspace using the Catkin tool.
Code Block |
---|
|
catkin_init_workspace |
- Compile.
Code Block |
---|
|
cd ..
catkin_make |
- Set up workspace environment.
Code Block |
---|
|
source devel/setup.bash |
- Launch the slamware_ros_sdk_server_node node. Select the corresponding IP according to the mode.
Code Block |
---|
|
roslaunch slamware_ros_sdk slamware_ros_sdk_server_node.launch ip_address:=10.6.128.141 // Station mode
// If in AP mode, the IP address is 192.168.11.1 |
- Open another terminal, repeat step 5, and start the sync_get_stcm_node node.
Code Block |
---|
|
roslaunch slamware_ros_sample sync_get_stcm.launch
// In the launch file, there is a default definition for the map_file_name parameter, indicating the path and filename where the map is saved. you can adjust parameters manually. |
- At this point, observe under slamware_ros_sample, a folder named 'map' will be generated, containing a file named 'data.map'.
Code Description
Code Block |
---|
language | cpp |
---|
title | sync_get_stcm |
---|
|
int main (int argc, char **argv)
{
std::string map_file_name;
ros::init(argc, argv, "sync_set_stcm_node");
ros::NodeHandle nh("~");
ros::ServiceClient client = nh.serviceClient<slamware_ros_sdk::SyncGetStcm>("/slamware_ros_sdk_server_node/sync_get_stcm");
slamware_ros_sdk::SyncGetStcm srv;
//get file name from paramter server
if (!nh.getParam("map_file_name",map_file_name))
{
ROS_ERROR("invalied file path......");
return 1;
}
//call service
if (client.call(srv))
{
ROS_INFO("get raw_stcm data success,writing to file......");
//check whether the target folder exists. create one if not
std::string dir;
dir = map_file_name.substr(0,map_file_name.rfind("/"));
if(access(dir.c_str(),0))
{
std::string cmd = "mkdir -p " + dir;
system(cmd.c_str());
}
std::ofstream fout(map_file_name, std::ios::out | std::ios::binary);
fout.write(reinterpret_cast<char *>(srv.response.raw_stcm.data()),(srv.response.raw_stcm.size()) * sizeof(srv.response.raw_stcm.front()));
fout.close();
ROS_INFO("raw_stcm data size: %zu",srv.response.raw_stcm.size());
ROS_INFO("save map at %s success......",map_file_name.c_str());
}
else
{
ROS_ERROR("Failed to get raw_stcm data......");
return 1;
}
return 0;
} |