This page introduces the usage of set_initial_pose, including how to use 2D Pose Estimate in RVIZ to set the pose of the robot.
...
Contents
...
Environment Setup
software platform
- Ubuntu 20.04 X86
- ROS Noetic
hardware platform
Choose any one below:
- Slamware Kit (User Robot System based on Slamware Solution)
- robot base systems like Apollo/Ares/Athena
...
Sample Code Download
ROS-Sample Download Link
...
Compile and Run
- Download the Slamware ROS SDK along with ROS examples.
- Place the 'src' folder from the ROS SDK into an empty working directory, such as 'catkin_ws'. Also, put the 'slamware_ros_sample' folder from the ROS examples into the 'src' folder.
Code Block |
---|
|
mkdir -p catkin_ws/src
cd catkin_ws/src |
- Initialize the workspace using the Catkin tool.
Code Block |
---|
|
catkin_init_workspace |
- Compile.
Code Block |
---|
|
cd ..
catkin_make |
- Set up workspace environment.
Code Block |
---|
|
source devel/setup.bash |
- Launch the slamware_ros_sdk_server_node node. Select the corresponding IP according to the mode.
Code Block |
---|
|
roslaunch slamware_ros_sdk slamware_ros_sdk_server_node.launch ip_address:=10.6.128.141 // Station mode
// If in AP mode, the IP address is 192.168.11.1 |
- Open another terminal, repeat step 5, and start the view_slamware_ros_sdk_server_node node.
Code Block |
---|
|
roslaunch slamware_ros_sdk view_slamware_ros_sdk_server_node.launch |
- Open another terminal, repeat step 5, and start the set_initial_pose_node node.
Code Block |
---|
|
roslaunch slamware_ros_sample set_initial_pose.launch |
- Click on '2D Pose Estimate' in RVIZ, then left-click on the desired location in the interface where you want to set the position of the car. While holding the left mouse button, move to change the angle. Once you release the mouse button, the pose is successfully set.
In the image below, the left side shows the effect before setting, and the right side shows the effect after setting.
Image Added
Image Added
...
Code Description
Code Block |
---|
language | cpp |
---|
title | Declare a global Publisher variable |
---|
|
ros::Publisher set_pose_pub; |
Code Block |
---|
language | cpp |
---|
firstline | 1 |
---|
title | Initialize the node and define publisher and subscriber variables |
---|
|
ros::init(argc, argv, "set_initial_pose_node");
ros::NodeHandle nh("~");
set_pose_pub = nh.advertise<geometry_msgs::Pose>("/slamware_ros_sdk_server_node/set_pose", 10);
ros::Subscriber initial_pose_sub = nh.subscribe("/initialpose", 10, initialPoseCallback); |
Code Block |
---|
language | cpp |
---|
title | Upon receiving the initialpose message, print out the message content, and then publish it |
---|
|
void initialPoseCallback(const geometry_msgs::PoseWithCovarianceStamped& msg)
{
ROS_INFO("receive initialpose: ");
ROS_INFO("position(xyz): %.3f %.3f %.3f", msg.pose.pose.position.x
, msg.pose.pose.position.y
, msg.pose.pose.position.z);
ROS_INFO("orientation(xyzw): %.3f %.3f %.3f %.3f", msg.pose.pose.orientation.x
, msg.pose.pose.orientation.y
, msg.pose.pose.orientation.z
, msg.pose.pose.orientation.w);
geometry_msgs::Pose _pose_msg(msg.pose.pose);
set_pose_pub.publish(_pose_msg);
} |