Versions Compared

Key

  • This line was added.
  • This line was removed.
  • Formatting was changed.

...

  1. Download the Slamware ROS SDK along with ROS examples.
  2. Place the 'src' folder from the ROS SDK into an empty working directory, such as 'catkin_ws'. Also, put the 'slamware_ros_sample' folder from the ROS examples into the 'src' folder.
    Code Block
    languagebash
    mkdir -p catkin_ws/src
    cd catkin_ws/src
  3. Initialize the workspace using the Catkin tool.
    Code Block
    languagebash
    catkin_init_workspace
  4. Compile.
    Code Block
    languagebash
    cd ..
    catkin_make
  5. Set up workspace environment.
    Code Block
    languagebash
    source devel/setup.bash

  6. Launch the slamware_ros_sdk_server_node node. Select the corresponding IP according to the mode.
    Code Block
    languagecpp
    roslaunch slamware_ros_sdk slamware_ros_sdk_server_node.launch ip_address:=10.6.128.141    // Station mode
    // If in AP mode, the IP address is 192.168.11.1
  7. Open another terminal, repeat step 5, and start the view_slamware_ros_sdk_server_node node.
    Code Block
    languagebash
    roslaunch slamware_ros_sdk view_slamware_ros_sdk_server_node.launch
  8. Open another terminal, repeat step 5, and start the display_virtual_lines_node node.
    Code Block
    languagebash
    roslaunch slamware_ros_sample display_virtual_lines.launch
  9. Configure and add the display of Marker information in Rviz.: 
    Click 'Add' in the bottom-left corner of Rviz, then in the pop-up window, select 'Marker' and click 'OK'. Upon success, as shown in the image below, a Marker is added to Displays, and the virtual walls are also displayed in the interface.

...